Liberty Lines commissions first high-speed ferry with mtu hybrid system from Rolls-Royce
Posted on June 28, 2024
- "Vittorio Morace" the world's first hybrid high-speed ferry to IMO HSC standard with a length of almost 40 metres is fast at sea and emission-free in harbour
- A further 8 Liberty Lines ferries with mtu hybrid systems will enter into service in Italy, Slovenia and Croatia
On 27 June 2024, the Italian shipping company Liberty Lines ceremonially launched the world's first hybrid fast ferry of this category and size in Trapani, Sicily, powered by an mtu hybrid propulsion system from Rolls-Royce. The 39.5 meter long ship has a capacity of 251 passengers, reaches a speed of over 30 knots and will significantly reduce the impact of ship operations on the environment. The "Vittorio Morace", built by the Spanish shipyard Astilleros Armon and designed by Incat Crowther, is the world's first IMO HSC (High-Speed Craft) hybrid fast ferry of this size and has been classified as a “Green Plus” ship by the Italian classification society RINA.
The new member of the fleet, named after the founder of the shipping company, is the first of nine ferries that will operate between Sicily and the neighbouring Aeolian and Egadi islands as well as between the Italian mainland, Croatia and Slovenia.
The battery-electric part of the drive is used for locally emission-free driving in the harbour area and as a booster. CO2 emissions are reduced by the particularly efficient mtu Series 4000 diesel engines which can also run on the renewable diesel (HVO, hydrotreated vegetable oil). Its use can lower the CO2 footprint by up to 90 per cent. Furthermore, the comparatively low overall weight of both the engines and the hybrid drive system contributes to high vessel propulsion efficiency, thereby reducing fuel consumption and emissions.
No compromises on speed and range, yet environmentally friendly
Gennaro Carlo Cotella, CEO of Liberty Lines, says: "We chose mtu hybrid systems because we want to minimise the environmental impact of our new fleet while not compromising on the high speed and range of our vessels. As we have trusted mtu products for decades, we have also opted for this partnership for our major fleet renewal.”
31 Liberty Lines ferries are a lifeline for the inhabitants of the Sicilian archipelago
The 31 ferries in the Liberty Lines fleet operate all year round, transporting more than three and a half million passengers on routes of up to 100 nautical miles. They not only serve as tourist excursion ships but are above all an important lifeline for many residents of the islands who have to commute regularly. The best known are the Aeolian Islands of Panarea, Stromboli, Vulcano, Alicudi, Filicudi, Lipari and Salina, which are UNESCO World Heritage Sites.
Denise Kurtulus, Vice President Global Marine at Rolls-Royce Power Systems says: "Liberty Lines is the ideal partner to demonstrate the progress that can be made towards environmentally and climate-friendly ship operation: We have used all possibilities and combined highly efficient combustion engines with exhaust gas aftertreatment, batteries and electric motors with an intelligent electronic control system to create an emission-optimised system. Together with Liberty Lines, Armon and Incat Crowther, we have developed a passenger ferry that will set new standards in this category of shipbuilding. We are proud of this. Our goal is to help this technology achieve a breakthrough.” The Marine business is one of the five key strategic initiatives presented by the Power Systems division at the Rolls-Royce Capital Markets Day in November 2023.
Automation and monitoring: mtu NautIQ Blue Vision NG and mtu NautIQ Foresight
All components are coordinated by the mtu NautIQ Blue Vision NG control and monitoring system. The complete propulsion systems of the first two ships will be monitored by the mtu NautIQ Foresight equipment health monitoring system. It collects data on the technical condition and analyses and stores it in order to improve the operational availability of the ship, reduce maintenance costs and lower fuel consumption and thus CO2 emissions.
How does the mtu hybrid propulsion system work?
When entering and leaving the port areas, the batteries ensure silent and emission-free manoeuvring. They supply power to all the ship's electrical equipment and the bow thrusters. When the ship leaves the harbour and increases speed, the mtu combustion engines are used. They drive the propellers directly, enabling the ship to travel at speeds of up to 30 knots. At the same time, they drive the hybrid electric motors via the gearboxes to charge the batteries and supply the electrical consumers on board without having to operate gensets. The generators on board are available as a backup. When the ship is in harbour, the batteries are used for the entire electrical supply on board during shorter stopovers, also silently and emission-free without power generators. During longer stopovers, shore power can be connected to recharge the batteries.
Technical data mtu Hybrid PropulsionPacks for Liberty Lines ferries:
Combustion Engines: 2 x mtu 16V4000 M65L, rated at 2560 kW @ 1800 rpm. IMO Tier III and US EPA Tier 4 emission compliant, together with mtu SCR exhaust after-treatment systems
Gearboxes: Reintjes WVSA-1542 hybrid-capable with clutchable PTO/PTIs for interfacing with Electric Machines
Electric Machines: 2 x Danfoss Editron EM-PMI375 T1100-2900 permanent magnet E-Machines. Providing in this case about 130 kW each of propulsion power, and when in charging mode up to about 260 kW each. By using variable speed electric motors, it allows the use of simple fixed pitch propellers for the vessel.
Generator Sets: 2 x 100 kWe variable-speed gensets, operating from 1000 - 2400 rpm, with lightweight PM generators
Batteries: 3 x 11 EST Green Orca 1050 Battery Packs (346 kWh total installed)
DC Switchboards (incl. DC power converters, circuit breakers, filters and protection equipment)
Electrical Power Management System
mtu NautIQ Blue Vision NG_Hybrid Control and Monitoring System - controlling and monitoring the complete Hybrid Propulsion system, and also the main ship systems (such as tanks, bilge alarms, gensets, etc.)
About Rolls-Royce Holdings plc
- Rolls-Royce develops and delivers complex power and propulsion solutions for safety-critical applications in the air, at sea and on land. Our products and service packages enable our customers to connect people, societies, cultures and economies together; they meet the growing need for power generation across multiple industries; and enable governments to equip their armed forces with the power to protect.
- Rolls-Royce has a presence in 48 countries and customers in more than 150, comprising over 250 commercial large aero engine customers, 160 armed forces and navies and approximately 40,000 active Power Systems customers. We are committed to becoming a net zero company by 2050 and we support our customers to do the same.
- Annual underlying revenue was £15.4bn in 2023, underlying operating profit was £1.6bn and free cash flow £1.3bn.
- Rolls-Royce Holdings plc is publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,500 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Contact
Phone: |
+49 7541 90 2159
|
E-mail: |