PRESS RELEASE Corporate

mtu unveils new automation system and restyled bridge components

Posted on October 05, 2012

Tognum subsidiary MTU Friedrichshafen GmbH will be presenting its Blue Vision New Generation automation system at the Salone Nautico Internazionale yacht show in Genoa from October 6 to 14 (Piazzale Marina scoperta, booth F2).

Images [2 Files, 2 MB]

  • Blue Vision New Generation automation system for mtu Series 2000 and 4000 engines
  • New bridge components designed by Pininfarina

Friedrichshafen/Genoa, October 5, 2012. Tognum subsidiary MTU Friedrichshafen GmbH will be presenting its Blue Vision New Generation automation system at the Salone Nautico Internazionale yacht show in Genoa from October 6 to 14 (Piazzale Marina scoperta, booth F2). It is an automation system for the monitoring and remote control of propulsion systems based on mtu Series 2000 or 4000 engines. The system will be available in a simple, non-classifiable version called Blue Vision Basic New Generation and in an expanded classifiable version called Blue Vision Advanced New Generation. At a later stage of development, Blue Vision Premium New Generation will represent the most comprehensive system. The new automation system   is currently undergoing sea trials in a 34-m yacht made by the Italian yacht builder Sanlorenzo. The SL 104 semi-displacement yacht is also on show in Genoa (at berth pier F) and is propelled by twin 16V 2000 M93 engines from mtu, each delivering 1,790kW power output.

Also being showcased by mtu is a yacht control stand with a design study of new bridge components. Equipment such as control levers, displays, operating consoles and instruments have been styled by Italian designer Pininfarina. With its standard, smooth new look for these components, mtu is responding to the exclusive requirements of yacht owners. The Pininfarina-designed equipment can be integrated into any yacht control stand, and is therefore also suitable for modular-built series yachts. It is also to be made compatible with mtu’s Blue Vision New Generation automation system.
Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: